Product Fact Sheets
The InfiniiVision 3 000G X-Series Oscilloscope: The Best in Usability Deserves the Best Features
Keysight’s InfiniiVision 3000G X-Series Oscilloscope offers high-end technology in a small form factor; equipping customers with a designed-for-touch user interface, industry-leading waveform update rate, and a multitude of powerful standard features. While the InfiniiVision 3000T was an outstanding general-purpose oscilloscope, the new InfiniiVision 3000G takes its performance up a notch. With 8 standard features customers previously had to upgrade to on the 3000T, including new waveform and measurement histograms, the 3000G is the clear winner in extended test capability. From R&D and debug requirements, to low-speed serial design and test, to even education needs– the 3000G equips you with the best available tools to support a diverse array of oscilloscope needs.
Benefits of the Keysight InfiniiVision 3000G oscilloscope over the InfiniiVision 3000T
The 3000G has extended test capability —with the best new features STANDARD
• Waveform and measurement histograms
• Built-in waveform generator
• I2C, SPI, UART, I2S, and USB PD trigger & decode
• Mask limit testing
• Measurement limit testing
• Frequency response analysis (Bode plots)
• Enhanced HDTV video analysis
• LAN/VGA connectivity module
The 3000G is the best-value option
• Features that extend test capability come standard
• Get the newest model with the best features for a fraction of the price of adding equivalent options to the 3000T
The 3000G enables ease of ordering
• No need to anticipate optional feature requirements you may need in the future– with the 3000G the features come standard
何をお探しですか?