Characterizing Superconducting Qubits

アプリケーションノート

Using AWG and digitizer setup controlled by Labber

Over the past two decades, superconducting quantum circuits have transitioned from basic research into a prominent industrial and academic platform for quantum computers. Subsequent improvements in coherence times, gate fidelities, and scalability have also motivated hardware manufacturers to enter into the quantum ecosystem. By supplying classical control hardware tailored towards quantum applications, engineers are enabled to push the quantum processor performance to higher levels. In this application note, we provide a brief introduction to the PXI-based quantum engineering tool-kit from Keysight, used to control and readout a single transmon qubit. We will also show how the hardware can be controlled and automated using our Labber software.