The Ixia Difference in Virtualization Testing

白書

With the deluge of data and devices growing, many service providers (SPs) see virtualized information technology (IT) infrastructures and virtual network functions (VNFs) as the keys to reclaim efficiencies. As they go down that path, knowing what lies ahead when conducting virtualization deployment testing can make all the difference.

Traditionally, SPs test in isolation, with dedicated testing for dedicated solutions—first in the pre-deployment lab. Then, on to production. Now, driven by the need to speed up deployment of new network services, they are changing their approach—to one that centers on continuous integration/ continuous deployment (CI-CD).