Enabling Next-Generation Automotive ADAS Cameras and Sensors with Automotive SerDes

White Paper

It is no secret that the pace of innovation in the automotive industry is exploding. If the last 20 years have been linear in the development of electrification, the previous two to three years have been exponential.

It used to be that a car was a means of getting from A to B. Now, we can safely say that is not true for today’s vehicles and certainly not for the new vehicles of tomorrow. Almost every new car on the market has a backup camera, park assist, and blind spot monitoring. Some offer a 360-degree view. Other features provide real-time traffic updates and a cellular connection to potential hazards, other road users, vehicles, or pedestrians. Some features can detect distracted or tired driving. Meanwhile, the people in the car are often unaware of driving conditions while they enjoy infotainment systems. Sensors, cameras, and networks enable these features.