Choose a country or area to see content specific to your location
應用說明
In digital circuits, insulating dielectrics separate the conducting parts (wire interconnects and transistors) from one another. As components have scaled and transistors have gotten closer and closermtogether, the insulating dielectrics have thinned to the point where charge build up and crosstalk adversely affect the performance of the device. It is this reduction in scale which drives the need for insulating materials with lower dielectric constant. A ‘low-k’ material is one with a small value for dielectric constant relative to silicon dioxide (SiO2)—a former dielectric of choice. The dielectric constant of SiO2 is 3.9. This number is the ratio of the permittivity of SiO2 divided by permittivity of vacuum, eSiO2/∈0,where ∈0 = 8.854 x 10-6 pFμm. There are many materials with lower dielectric constants, but few of them can be suitably integrated into a semiconductor manufacturing process[1].
解鎖內容
免費註冊
*Indicates required field
感謝您!
您的表格已成功送出
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
請銷售人員與我聯絡。
*Indicates required field
感謝您!
A sales representative will contact you soon.