What are you looking for?
PathWave Digital Pre-Distortion (DPD) Explorer
Digital Pre-Distortion (DPD) is one of the most fundamental analyses in wireless communication systems. It helps to increase the efficiency of Power Amplifiers (PAs) by reducing the distortion created by running PAs in their non-linear regions. PathWave DPD Explorer captures amplifier nonlinearity and creates pre-distortion algorithms and settings for the linearization of cellular and WiFi systems.
The DPD Explorer user interface (UI) :
- Enables engineers to configure various signal formats and DPD algorithms quickly and conveniently
- Supports common communication signal formats, such as 5G NR, LTE, WLAN, and I/Q user definitions
- Supports a new Dynamic Gain algorithm for extracting the parameters of PAs with memory and trap effects
- Includes a Direct DPD method which shows the theoretical limit of DPD comparison between different PA models
- Supports classical DPD parameter identification methods, such as Memory Polynomial, Volterra Polynomial, and Look-Up Table
DPD Explorer 2024
DPD Explorer 2024 is the first version to be supported on both the Windows and Linux platforms.
DPD Explorer 2024 Compatibility
The following table lists DPD Explorer 2024 compatible versions of ADS.
DPD Explorer Versions | ADS Versions |
---|---|
|
|
DPD Explorer 2024 Installation
DPD Explorer is a plugin for ADS that is installed during or after System Design installation.
Documentation
Install DPD Explorer
DPD Explorer is a plugin for ADS that is installed during or after System Design installation.
On Windows
DPD Explorer can be installed using the following methods:
- During the PathWave System Design installation.
While installing System Design, select Add System Design tools to ADS.
- After PathWave System Design Installation.
1. Open System Design and load a blank workspace.
2. Click Tools > Install System Design Addon in ADS.
3. If prompted, select the ADS version and click OK.
Upon successful installation, the DPD Explorer option is added to the Tools menu in the Schematic Window.
On Linux
Prerequisite:
- Install dotnet 6.0. For more information, see https://access.redhat.com/documentation/en-us/net/6.0.
- Download System Design Linux Installer, See PathWave System Design HPC.
- After the download, unzip or untar the installer file using the command:
tar -xzf <tar.gz>
- Copy the following two binary files from
<SystemDesign_install_dir>
/SystemDesignInADS/<ADS_release>
/bin
to the ADS bin directory.
-SystemVueDpdIPCRouter
-SystemVueDpdServer
<SystemDesign_install_dir> is the System Design installation directory on Linux. - In ADS App Manager, click the Add User ADS Addon button and point to:
SystemDesignInADS/ael/SystemDesignStartup.atf
Note: Do not move the SystemDesignStartup.atf
file
Upon successful configuration, the DPD Explorer command is available in the Tools menu of the ADS schematic window.
DPD Explorer 2023 Update 0.1
DPD Explorer 2023 Update 0.1 Compatibility
The following table lists DPD Explorer 2023 Update 0.1 compatible versions of ADS.
DPD Explorer Versions | ADS Versions |
---|---|
|
|
DPD Explorer 2023 Update 0.1 Installation
Platform |
Filename | Downloads | Size |
---|---|---|---|
Windows 64-bit | dpdexplorerInADS_2023_update0.1_shp_win_x64.exe |
Download | 734,003,200 bytes (700 MB) |
Note: DPD Explorer is supported on Linux starting with DPD Explorer 2024. DPD Explorer 2023 Update 0.1 is not supported with ADS 2024 or later versions.
Documentation
Install DPD Explorer
Installation Instructions:
- Download the DPD Explorer installer.
- Run the installer and follow the wizard.
Note: If you have DPD Explorer 2023 installed, please uninstall it before installing 2023 Update 0.1.
DPD Explorer 2023
DPD Explorer 2023 Compatibility
The following table lists DPD Explorer 2023 compatible versions of ADS.
DPD Explorer Versions | ADS Versions |
---|---|
|
|
DPD Explorer 2023 Installation
Platform |
Filename | Downloads | Size |
---|---|---|---|
Windows 64-bit | dpdexplorerinADS_2023_shp_win_x64.exe |
Download | 742,391,808 bytes (708 MB) |
Note: DPD Explorer is supported on Linux starting with DPD Explorer 2024.
Documentation
Install DPD Explorer
DPD functionality is available as a separate add-on. You need to download the installation package and install it along with your ADS instance.
On Windows
After the download, run the DPD Explorer installer and follow the instructions.
Return to the Advanced Design System (ADS) Software downloads page.