Keysight Digital Pre-Distortion (DPD) is one of the most fundamental analyses in wireless communication systems. It helps to increase the efficiency of Power Amplifiers (PAs) by reducing the distortion created by running PAs in their non-linear regions. PathWave DPD Explorer captures amplifier nonlinearity and creates pre-distortion algorithms and settings for the linearization of cellular and WiFi systems.

The DPD Explorer user interface (UI) :

  • Enables engineers to configure various signal formats and DPD algorithms quickly and conveniently
  • Supports common communication signal formats, such as 5G NR, LTE, WLAN, and I/Q user definitions
  • Supports a new Dynamic Gain algorithm for extracting the parameters of PAs with memory and trap effects
  • Includes a Direct DPD method which shows the theoretical limit of DPD comparison between different PA models
  • Supports classical DPD parameter identification methods, such as Memory Polynomial, Volterra Polynomial, and Look-Up Table

Modulation Explorer

The Modulation Explorer enables circuit designers to analyze the modulated performance of their RFIC designs and optimize them in ADS, ensuring both performance and compliance. It supports nearly all communication signal formats, including 5G NR, LTE, WLAN, and I/Q user definitions.

Modulation and DPD Explorer 2026

Modulation and DPD Explorer 2026 Compatibility

The following table lists Modulation and DPD Explorer 2026 compatible versions of ADS.

Modulation and DPD Explorer Versions ADS Versions
  • 2026
  • ADS 2026 Update 0.1, Update 1.0, Update 1.1, Update 1.2
  • ADS 2026
  • ADS 2025 Update 2.0, Update 2.1, Update 2.2, Update 2.3
  • ADS 2025 Update 1.0, Update 1.1
  • ADS 2025

Modulation and DPD Explorer 2026 Installation

Modulation and DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

Documentation

Modulation and DPD Explorer 2026 Release Notes

Modulation and DPD Explorer Product Documentation

Install DPD Explorer

On Linux

Prerequisite:

Install dotnet 8.0. For more information, see https://docs.redhat.com/en/documentation/net/8.0 and make sure the dotnet path is set.

$ export DOTNET_ROOT=<PATH to DOTNET Installation>

$ export PATH=$PATH:$DOTNET_ROOT:$DOTNET_ROOT/tools

Note:

  •  DotNet 8 is required for Modulation & DPD Explorer, hence RHEL 7 is not supported. 
  • On Linux, the environment variable LANG should be set to en_US.UTF-8.
  • On Linux, Modulation & DPD Explorer has a dependency on libncurses5, make sure this library is installed and the installation location is part of LD_LIBRARY_PATH.
  • If the legacy module libncurses5 is not available, you could create a softlink in the SystemVue lib directory: ln -s /lib64/libncurses.so.6 libncurses.so.5

Download SystemVue 2026 Digital Pre-Distortion (DPD) Explorer and Modulation Explorer Linux Installer

SHA256: E5990F2D4BC2284E8B1B19D0352B4ACA7E16254ABB8454068114556AA4832385

1. After the download, unzip or untar the installer file using the command

tar -xzf <tar.gz>

2. Copy the following two binary files from 

<SystemVue_Install_DIR>/SystemVueEXP/<version>/SystemDesignInADS/<ADS_release_version_number>/bin

  • SystemVueDpdIPCRouter
  • SystemVueDpdServer

<SystemVue_Install_DIR>/SystemVueEXP/<version> is the Modulation & DPD Explorer installation directory on Linux.

Note: If you want to you install Modulation & DPD Explorer with respect to ADS. <ADS_release_version_number>, ADS version should be the same or previous ADS version. For example:

  • If your ADS version is 2026 U1 then you should pick up the previous ADS version which is ADS 2026.
  • If your ADS version is 2025 U2.1 then you should pick up the previous ADS version which is ADS 2025U2.

3. Paste the copied binary files into the ADS bin directory.

4. In ADS App Manager, click the "Add User ADS Addon" button and point to:

<SystemVue_Install_DIR>/SystemDesignInADS/ael/SystemDesignStartup.atf

Note: Do not move the SystemDesignStartup.atf file.

On successful configuration, the Modulation & DPD Explorer command is available in the Tools menu of the ADS schematic window.

Modulation and DPD Explorer 2025 Update 1.0

Modulation and DPD Explorer 2025 Update 1.0 Compatibility

The following table lists Modulation and DPD Explorer 2025 compatible versions of ADS. 

Modulation and DPD Explorer Versions ADS Versions
  • 2025 Update 1.0
  • 2024
  • 2024 Update 1.0, 1.1, 1.2
  • 2024 Update 2.0, 2.1, 2.2
  • 2025
  • 2025 Update 1.0
  • 2025 Update 2.0
  • 2026 Update 0.1
  • 2026 Update 1.0

Modulation and DPD Explorer 2025 Update 1.0 Installation

Modulation and DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

Documentation

Install DPD Explorer

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

On Windows

DPD Explorer can be installed using the following methods:

  • During the System Design installation.
    While installing System Design, select Add System Design tools to ADS.
  • After System Design Installation.
    1. Open System Design and load a blank workspace.
    2. Click Tools > Install System Design Addon in ADS.
    3. If prompted, select the ADS version and click OK.

Upon successful installation, the DPD Explorer option is added to the Tools menu in the Schematic Window.

On Linux

SHA256: B29D045304249E936007349F3A619DDC5BDA2B34C2902ECBEEC8388ED4581898

  1. After the download, unzip or untar the installer file using the command: 
       tar -xzf <tar.gz>
  2. Copy the following two binary files from
       <SystemDesign_install_dir>/SystemDesignInADS/<ADS_release>/bin
    to the ADS bin directory.
       - SystemVueDpdIPCRouter
       - SystemVueDpdServer
    <SystemDesign_install_dir> is the System Design installation directory on Linux.
  3. In ADS App Manager, click the Add User ADS Addon button and point to:
       SystemDesignInADS/ael/SystemDesignStartup.atf

Note: Do not move the SystemDesignStartup.atf file

Upon successful configuration, the DPD Explorer command is available in the Tools menu of the ADS schematic window.

Modulation and DPD Explorer 2025 Update 0.1

Modulation and DPD Explorer 2025 Update 0.1 Compatibility

The following table lists Modulation and DPD Explorer 2025 compatible versions of ADS. 

Modulation and DPD Explorer Versions ADS Versions
  • 2025 Update 0.1
  • 2023
  • 2023 Update 1.0
  • 2023 Update 2.0
  • 2024
  • 2024 Update 1.0, 1.1, 1.2
  • 2024 Update 2.0, 2.1, 2.2
  • 2025
  • 2025 Update 1.0
  • 2025 Update 2.0

Modulation and DPD Explorer 2025 Update 0.1 Installation

Modulation and DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

Documentation

Install DPD Explorer

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

On Windows

DPD Explorer can be installed using the following methods:

  • During the System Design installation.
    While installing System Design, select Add System Design tools to ADS.
  • After System Design Installation.
    1. Open System Design and load a blank workspace.
    2. Click Tools > Install System Design Addon in ADS.
    3. If prompted, select the ADS version and click OK.

Upon successful installation, the DPD Explorer option is added to the Tools menu in the Schematic Window.

On Linux

Prerequisite:

Note: 
- DotNet 8 is required for DPD Explorer, hence RHEL 7 is not supported. 
- On Linux, the environment variable LANG should be set to en_US.UTF-8.
- On Linux, DPD Explorer has a dependency on libncurses5, make sure this library is installed and the installation location is part of LD_LIBRARY_PATH.
- If the legacy module libncurses5 is not available, you could create a softlink in the SystemVue lib directory:
  ln -s /lib64/libncurses.so.6 libncurses.so.5

  1. After the download, unzip or untar the installer file using the command: 
       tar -xzf <tar.gz>
  2. Copy the following two binary files from
       <SystemDesign_install_dir>/SystemDesignInADS/<ADS_release>/bin
    to the ADS bin directory.
       - SystemVueDpdIPCRouter
       - SystemVueDpdServer
    <SystemDesign_install_dir> is the System Design installation directory on Linux.
  3. In ADS App Manager, click the Add User ADS Addon button and point to:
       SystemDesignInADS/ael/SystemDesignStartup.atf

Note: Do not move the SystemDesignStartup.atf file

Upon successful configuration, the DPD Explorer command is available in the Tools menu of the ADS schematic window.

DPD Explorer 2024 Update 2.0

DPD Explorer 2024 Update 2.0 Compatibility

The following table lists DPD Explorer 2024 Update 2.0 compatible versions of ADS. 

DPD Explorer Versions ADS Versions
  • 2024 Update 2.0
  • 2023
  • 2023 Update 1.0
  • 2023 Update 2.0
  • 2024
  • 2024 Update 1.0, 1.1, 1.2
  • 2024 Update 2.0, 2.1, 2.2
  • 2025

DPD Explorer 2024 Update 2.0 Installation

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

Documentation

Install DPD Explorer

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

On Windows

DPD Explorer can be installed using the following methods:

  • During the PathWave System Design installation.
    While installing System Design, select Add System Design tools to ADS.
  • After PathWave System Design Installation.
    1. Open System Design and load a blank workspace.
    2. Click Tools > Install System Design Addon in ADS.
    3. If prompted, select the ADS version and click OK.

Upon successful installation, the DPD Explorer option is added to the Tools menu in the Schematic Window.

On Linux

Prerequisite:

Note: 
- DotNet 8 is required for DPD Explorer, hence RHEL 7 is not supported. 
- On Linux, the environment variable LANG should be set to en_US.UTF-8.
- On Linux, DPD Explorer has a dependency on libncurses5, make sure this library is installed and the installation location is part of LD_LIBRARY_PATH.
- If the legacy module libncurses5 is not available, you could create a softlink in the SystemVue lib directory:
  ln -s /lib64/libncurses.so.6 libncurses.so.5

  1. After the download, unzip or untar the installer file using the command: 
       tar -xzf <tar.gz>
  2. Copy the following two binary files from
       <SystemDesign_install_dir>/SystemDesignInADS/<ADS_release>/bin
    to the ADS bin directory.
       - SystemVueDpdIPCRouter
       - SystemVueDpdServer
    <SystemDesign_install_dir> is the System Design installation directory on Linux.
  3. In ADS App Manager, click the Add User ADS Addon button and point to:
       SystemDesignInADS/ael/SystemDesignStartup.atf

Note: Do not move the SystemDesignStartup.atf file

Upon successful configuration, the DPD Explorer command is available in the Tools menu of the ADS schematic window.

DPD Explorer 2024 Update 1.0

DPD Explorer 2024 is the next version to be supported on both the Windows and Linux platforms.

DPD Explorer 2024 Update 1.0 Compatibility

The following table lists DPD Explorer 2024 Update 1.0 compatible versions of ADS. 

DPD Explorer Versions ADS Versions
  • 2024 Update 1.0
  • 2023
  • 2023 Update 1.0
  • 2023 Update 2.0
  • 2024
  • 2024 Update 1.0, 1.1, 1.2
  • 2024 Update 2.0, 2.1, 2.2

DPD Explorer 2024  Update 1.0 Installation

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

Documentation

Install DPD Explorer

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

On Windows

DPD Explorer can be installed using the following methods:

  • During the PathWave System Design installation.
    While installing System Design, select Add System Design tools to ADS.
  • After PathWave System Design Installation.
    1. Open System Design and load a blank workspace.
    2. Click Tools > Install System Design Addon in ADS.
    3. If prompted, select the ADS version and click OK.

Upon successful installation, the DPD Explorer option is added to the Tools menu in the Schematic Window.

On Linux

Prerequisite:

  1. After the download, unzip or untar the installer file using the command: 
       tar -xzf <tar.gz>
  2. Copy the following two binary files from
       <SystemDesign_install_dir>/SystemDesignInADS/<ADS_release>/bin
    to the ADS bin directory.
       - SystemVueDpdIPCRouter
       - SystemVueDpdServer
    <SystemDesign_install_dir> is the System Design installation directory on Linux.
  3. In ADS App Manager, click the Add User ADS Addon button and point to:
       SystemDesignInADS/ael/SystemDesignStartup.atf

Note: Do not move the SystemDesignStartup.atf file

Upon successful configuration, the DPD Explorer command is available in the Tools menu of the ADS schematic window.

DPD Explorer 2024

DPD Explorer 2024 is the first version to be supported on both the Windows and Linux platforms.

DPD Explorer 2024 Compatibility

The following table lists DPD Explorer 2024 compatible versions of ADS. 

DPD Explorer Versions ADS Versions
  • 2024
  • 2023
  • 2023 Update 1.0
  • 2023 Update 2.0
  • 2024
  • 2024 Update 1.0
  • 2024 Update 2.0

DPD Explorer 2024 Installation

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

Documentation

Install DPD Explorer

DPD Explorer is a plugin for ADS that is installed during or after System Design installation.

On Windows

DPD Explorer can be installed using the following methods:

  • During the PathWave System Design installation.
    While installing System Design, select Add System Design tools to ADS.
  • After PathWave System Design Installation.
    1. Open System Design and load a blank workspace.
    2. Click Tools > Install System Design Addon in ADS.
    3. If prompted, select the ADS version and click OK.

Upon successful installation, the DPD Explorer option is added to the Tools menu in the Schematic Window.

On Linux

Prerequisite:

  1. After the download, unzip or untar the installer file using the command: 
       tar -xzf <tar.gz>
  2. Copy the following two binary files from
       <SystemDesign_install_dir>/SystemDesignInADS/<ADS_release>/bin
    to the ADS bin directory.
       - SystemVueDpdIPCRouter
       - SystemVueDpdServer
    <SystemDesign_install_dir> is the System Design installation directory on Linux.
  3. In ADS App Manager, click the Add User ADS Addon button and point to:
       SystemDesignInADS/ael/SystemDesignStartup.atf

Note: Do not move the SystemDesignStartup.atf file

Upon successful configuration, the DPD Explorer command is available in the Tools menu of the ADS schematic window.

DPD Explorer 2023 Update 0.1

DPD Explorer 2023 Update 0.1 Compatibility

The following table lists DPD Explorer 2023 Update 0.1 compatible versions of ADS.

DPD Explorer Versions ADS Versions
  • 2023 Update 0.1
  • 2022
  • 2022 Update 1.0
  • 2022 Update 2.0
  • 2023
  • 2023 Update 1.0
  • 2023 Update 2.0

DPD Explorer 2023 Update 0.1 Installation

Download the DPD Explorer 2023 Update 0.1
Platform
FilenameDownloadsSize
Windows 64-bitdpdexplorerInADS_2023_update0.1_shp_win_x64.exe
Download734,003,200 bytes (700 MB)

Note: DPD Explorer is supported on Linux starting with DPD Explorer 2024. DPD Explorer 2023 Update 0.1 is not supported with ADS 2024 or later versions.

Documentation

Install DPD Explorer

Installation Instructions:

  1. Download the DPD Explorer installer.
  2. Run the installer and follow the wizard.

Note: If you have DPD Explorer 2023 installed, please uninstall it before installing 2023 Update 0.1.

DPD Explorer 2023

DPD Explorer 2023 Compatibility

The following table lists DPD Explorer 2023 compatible versions of ADS.

DPD Explorer Versions ADS Versions
  • 2023
  • 2022
  • 2022 Update 1.0
  • 2022 Update 2.0
  • 2023
  • 2023 Update 1.0

DPD Explorer 2023 Installation

Download DPD Explorer 2023
Platform
FilenameDownloadsSize
Windows 64-bitdpdexplorerinADS_2023_shp_win_x64.exe
Download742,391,808 bytes (708 MB)

Note: DPD Explorer is supported on Linux starting with DPD Explorer 2024.

Documentation

Install DPD Explorer

DPD functionality is available as a separate add-on. You need to download the installation package and install it along with your ADS instance.

On Windows

After the download, run the DPD Explorer installer and follow the instructions.

Return to the Advanced Design System (ADS) Software downloads page.