何をお探しですか?
Armis
from SeviceNow
Armis from ServiceNow and Keysight: Real-time insight to Drive CTEM
Organizations today face the challenge of seeing and securing every connected device across IT, OT, IoT, and medical environments, while keeping infrastructure lean and efficient. Keysight and Armis have partnered to deliver an integrated solution that combines Keysight’s Vision E1S network packet brokers (NPBs) with the Armis Centrix™Collector. This joint offering eliminates the need for additional hardware while extending value beyond network visibility and security to include comprehensive Continuous Threat Exposure Management (CTEM) across all connected assets.
Enterprises Operate in Increasingly Complex Environments
The growth of connected devices, including physical, logical, and virtual, has expanded the attack surface to such a degree that it is increasingly hard to have situational awareness on all assets and their pathways, let alone secure them. SOC and IT leaders face a daunting list of challenges:
- Visibility gaps – Blind spots created by the combination of point security solutions and unmanaged or unknown devices leave organizations exposed.
- Escalating risks – Without clear context, incidents can rapidly escalate from minor issues to major breaches.
- Tool sprawl – Multiple security tools demand more infrastructure and often interoperate, creating operational inefficiencies, security blind spots, and higher costs.
- Resource constraints – Teams are leaner, often with limited time and expertise to address the growing volume of alerts.
- Pressure to consolidate – Organizations are seeking streamlined, integrated solutions to maximize ROI and reduce complexity.
Armis and Keysight have created a unified solution by embedding the Armis Centrix™ Collector directly into Keysight’s Vision E1S series network packet brokers. Instead of deploying additional hardware, organizations gain immediate access to Armis’s leading CTEM capabilities through their existing Keysight infrastructure.
Armis Advantage: How It Works
This integration ensures that both network security and cyber exposure management are delivered seamlessly from a single, consolidated footprint.
- Network Packet Broker Foundation – Keysight packet brokers efficiently aggregate, filter, and distribute network traffic.
- Embedded Armis Centrix Collector – The Armis Centrix™ Collector runs directly on the Vision E1S, eliminating the need for extra gear.
- Device Intelligence + CTEM – Armis ingests the data, applies advanced analytics and threat intelligence, to deliver complete device visibility, security and control of all assets.
- Actionable Insights – Security teams receive enriched context about every device, enabling faster response and proactive risk reduction.
Armis Centrix for Asset Management and Security
The video introduces Armis Centrix™, a cloud-native platform that provides full visibility into all IT, OT, IoT, and unmanaged assets. It passively discovers and classifies every device, detects anomalous or malicious behavior in real time, prioritizes remediation efforts based on risk, and integrates with existing security tools to enforce policy and reduce attack surface.
Visibility
Address the Continuous Threat Exposure Management Challenge:
Organizations get more value out of their visibility investments, while Armis delivers the intelligence needed to see, secure, and manage the entire attack surface. Together, Armis and Keysight empower enterprises to reduce complexity, cut costs, and strengthen cyber resilience.
This integrated approach addresses growing visibility gaps, tool sprawl, and resource constraints by combining Keysight’s trusted network packet broker technology with Armis’ advanced analytics and CTEM capabilities. Organizations gain real-time, agentless insight across IT, OT, IoT, and medical environments, enabling faster risk mitigation, streamlined operations, and improved ROI while reducing complexity and strengthening cyber resilience.
- Complete Visibility – Gain real-time visibility, security and control of all connected assets across IT, OT, IoT, and medical environments.
- Reduced Infrastructure – Eliminate the need for additional collectors or appliances.
- Faster, Smarter Decisions – With enriched Armis intelligence, security teams can respond to threats with speed and accuracy.
- Streamlined Operations – Simplify toolsets and reduce operational overhead by consolidating functions onto Keysight’s Vision E1S.
- Enhanced Value Proposition – Extend Keysight’s role in the enterprise from network security to full cyber exposure management.
Featured Resources
Want help or have questions?