What are you looking for?
Hawkeye
| リリース | バージョン | 内容 |
|---|---|---|
| 2026-10-26 | 6.1.1-101 | Hawkeye 6.1.1-101 is a General Availability release for new installs, It is distributed as an upgrade repository file running on Linux. Hawkeye Server 6.1.1 is a general availability release on the Debian 12 platform. Existing customers can look at the migration document for details on upgrading from 5.5.5 to 6.0.1 to 6.0.7-57 to 6.1.1. For New customers please use 6.1.1-101 distributed as an OVA or QCOW2. CRITICAL INFORMATION: Existing Customers should upgrade to 6.0.7-57 before going to 6.1.1-101. This build also contains key PHP Vulnerability fix as well. *VISION E1S will not be supported from Hawkeye 6.0.1 onwards. Customers who have Vision E1S connected to Hawkeye 5.5.5 - DO NOT UPGRADE – CONTACT CUSTOMER SUPPORT FOR MORE INFORMATION |
| リリース | バージョン |
|---|---|
| 2026-10-26 | 6.1.1-101 |
| Version Description |
|---|
| Hawkeye 6.1.1-101 is a General Availability release for new installs, It is distributed as an upgrade repository file running on Linux. Hawkeye Server 6.1.1 is a general availability release on the Debian 12 platform. Existing customers can look at the migration document for details on upgrading from 5.5.5 to 6.0.1 to 6.0.7-57 to 6.1.1. For New customers please use 6.1.1-101 distributed as an OVA or QCOW2. CRITICAL INFORMATION: Existing Customers should upgrade to 6.0.7-57 before going to 6.1.1-101. This build also contains key PHP Vulnerability fix as well. *VISION E1S will not be supported from Hawkeye 6.0.1 onwards. Customers who have Vision E1S connected to Hawkeye 5.5.5 - DO NOT UPGRADE – CONTACT CUSTOMER SUPPORT FOR MORE INFORMATION |
Hawkeye 6.1.1-101 is a General Availability release for new installs, It is distributed as an upgrade repository file running on Linux. Hawkeye Server 6.1.1 is a general availability release on the Debian 12 platform. Existing customers can look at the migration document for details on upgrading from 5.5.5 to 6.0.1 to 6.0.7-57 to 6.1.1. For New customers please use 6.1.1-101 distributed as an OVA or QCOW2. CRITICAL INFORMATION: Existing Customers should upgrade to 6.0.7-57 before going to 6.1.1-101. This build also contains key PHP Vulnerability fix as well.
*VISION E1S will not be supported from Hawkeye 6.0.1 onwards. Customers who have Vision E1S connected to Hawkeye 5.5.5 - DO NOT UPGRADE – CONTACT CUSTOMER SUPPORT FOR MORE INFORMATION
インストール方法
説明資料
ダウンロード
Hawkeye_6.1.1-100 256GB OVA
Hawkeye 6.1.1-100 256GB QCOW2
Hawkeye 6.1.1-100 offline Repo ISO
XR2000 Upgrade for IxChariot Customers Only NEED WORKING LINK
XRPi Upgrade for IxChariot Customers Only
Raspberry Pi4 Software Image
HDET Scripts
Hawkeye 6.0.7-57 is a General Availability release for new installs, It is distributed as an upgrade repository file running on Linux. Hawkeye Server 6.0.7-57 is a general availability release on the Debian 12 platform. Existing customers can look at the migration document for details on upgrading from 5.5.5 to 6.0.1 For New customers please use 6.0.7-57 distributed as an OVA or QCOW2.
CRITICAL INFORMATION: *VISION E1S will not be supported from Hawkeye 6.0.1 onwards. Customers who have Vision E1S connected to Hawkeye 5.5.5 - DO NOT UPGRADE – CONTACT CUSTOMER SUPPORT FOR MORE INFORMATION
インストール方法
説明資料
Hawkeye Server 6.0.7 release is a general availability release on a Debian 12 platform. Existing customers should
install the new 6.0.1 as a fresh install and follow the steps set in the migration document to migrate from Hawkeye
5.5.5 to Hawkeye 6.0.1. Customers then subsequently can upgrade to Hawkeye 6.0.7. Please note, that if you are in
any release before Hawkeye 5.5.5, please update to Hawkeye 5.5.5 before attempting the migration. For New
customers, an OVA or QCOW2 of 6.0.7 will be available to install.