Scaling Up AI Compute

白書

Artificial intelligence (AI) workloads are driving unprecedented demand for compute performance, memory bandwidth, and accelerator connectivity. As AI models grow larger and more complex, system performance increasingly depends not only on the capabilities of individual processors and accelerators, but also on how efficiently data moves throughout the infrastructure. The ability to transfer massive data sets between compute resources with minimal latency has become a critical factor in determining overall system utilization and scalability.

 

To address these requirements, the industry is expanding AI infrastructure through multiple complementary scaling approaches. Scale-in technologies improve performance within a device or package through innovations such as chiplets and high-bandwidth memory (HBM). Scale-out architectures connect compute resources across larger clusters using technologies such as Ethernet and InfiniBand. Between these approaches lies scale-up: the tightly coupled interconnection of processors, accelerators, memory resources, and switches within a server, rack, or rack-scale domain. By enabling high-bandwidth, low-latency communication among participating resources, scale-up architectures help maximize the effectiveness of available compute while addressing growing constraints on power, cooling, and physical footprint.

 

Three technology domains form the foundation of AI scale-up systems: compute input/output interfaces (I/O), memory technologies, and accelerator fabrics. Compute I/O standards such as Peripheral Component Interconnect Express (PCIe®️) and Compute Express Link (CXL®️) connect processors, accelerators, switches, and memory resources. Memory technologies, including Double Data Rate (DDR), Low-Power DDR (LPDDR), Graphics DDR (GDDR), and HBM, provide different balances of bandwidth, capacity, power consumption, and packaging efficiency. Accelerator fabrics, including Ultra Accelerator Link (UALink), NVLink, and emerging Ethernet-based scale-up approaches, enable high-speed communication among accelerators working on shared AI workloads.

 

As AI performance requirements continue to grow, each of these technology domains is evolving rapidly. PCIe 7.0 and CXL 4.0 increase available bandwidth and enable more advanced memory-access models. Next-generation memory technologies seek to deliver higher capacity and throughput while balancing power and system complexity. Accelerator fabrics continue to advance to support larger workloads distributed across increasing numbers of compute devices. Together, these technologies help remove performance bottlenecks and improve overall system efficiency, but they also introduce significant validation challenges.

 

Higher signaling rates, shrinking electrical margins, advanced equalization techniques, adaptive training mechanisms, and increasingly complex system architectures require more comprehensive validation methodologies than previous generations. Technologies such as PAM3 signaling, forward error correction, adaptive equalization, and coherency protocols create new interactions that must be understood and verified. Validation teams must characterize transmitter and receiver performance, evaluate channel behavior, and assess interoperability across a growing range of operating modes and deployment scenarios.

 

The challenge extends beyond demonstrating compliance with a specification. Standards compliance establishes a common baseline and confirms conformance to defined requirements, but it does not guarantee robust operation across all system configurations, environmental conditions, or interoperability scenarios. Devices that pass compliance testing may still encounter integration issues when interacting with specific link partners, training algorithms, traffic patterns, or topologies. As a result, engineering teams increasingly need validation strategies that connect compliance results with broader characterization and system-level testing.

 

This paper examines the role of validation in supporting reliable AI scale-up infrastructure. It explores the evolution of modern compute I/O, memory, and accelerator fabric technologies and explains the performance challenges driving the development of new standards. It also reviews common validation concerns, including channel loss, jitter, noise, crosstalk, equalization behavior, interoperability risk, and architectural diversity across AI platforms.

 

In addition, the paper discusses the importance of transmitter and receiver validation, operating-margin characterization, and integration testing as complementary elements of a complete validation methodology. Understanding available margin can help engineers evaluate design robustness, identify interoperability risks, and assess how systems may behave under changing environmental and operating conditions. As electrical budgets continue to tighten, margin characterization becomes increasingly important for predicting real-world reliability and reducing deployment risk.

 

Finally, the paper highlights the growing importance of repeatable workflows and test automation. As standards continue to evolve and validation coverage requirements expand, automated approaches can help teams improve consistency, reduce manual effort, and maintain traceability across projects and product generations. Scalable validation methodologies enable engineering teams to adapt to changing interface requirements while maintaining confidence in test results.

 

By connecting compliance, characterization, and system-level validation, engineering organizations can better understand how compute I/O, memory, and accelerator fabrics interact within modern AI infrastructures. These insights help teams identify limitations earlier in development, mitigate integration challenges, and build confidence that scale-up architectures will deliver the performance, reliability, and efficiency required by next-generation AI systems.