eBooks
We at Eggplant and the hundreds of thousands of Eggplant accredited engineers are on a mission to rid the world of bad software. We do so by allowing our diverse set of happy customers to test their applications and processes through the eyes of the user at speed and scale.
Eggplant is a non-invasive automation platform that can automate anything, is supercharged by Intelligence, and provides real-time monitoring on how your customers are using your product.
Eggplant automates any software such as Salesforce, WorkDay, Containerized Applications, and non-traditional user interfaces like Heads Up Displays.
何をお探しですか?