eBooks
Noise figure is one of the most important measurements for understanding how well a receiver, amplifier, converter, transistor, or complete RF system can process weak signals. In communication, radar, satellite, wireless, and microwave systems, the signal of interest often arrives at a low power level. Any noise added by the receiving chain can obscure that signal, reduce signal-to-noise ratio (SNR), and limit system sensitivity. This eBook, Learn the Fundamentals of Noise Figure Measurement, explains how noise figure characterizes that degradation and why accurate, repeatable noise figure measurements are essential for component and system evaluation.
The resource begins by defining noise figure as the ratio of signal-to-noise power at the input and output of a network. It explains that an ideal amplifier would increase the signal and input noise equally, preserving SNR, while a real amplifier adds noise from its own components and reduces the output SNR. The eBook connects noise figure with related system parameters such as sensitivity and bit error ratio (BER), showing why noise figure is often used to compare receiving systems, amplifiers, and transistors. Once noise figure is known, engineers can estimate system sensitivity from bandwidth and understand how individual devices contribute to total receiver performance.
The eBook also explains how noise figure applies to a cascade of devices. Using the Friis formula, engineers can calculate the total noise contribution of multiple stages when the gain and noise figure of each stage are known. The guide reinforces a practical signal-chain principle: the lowest-noise devices and highest-gain stages should be placed early in the chain because early-stage performance strongly influences the total system noise figure. This explanation is useful for RF front-end design, receiver chain optimization, amplifier selection, and system-level noise budgeting.
The asset covers two primary noise sources: thermal noise and shot noise. Thermal noise results from the motion of conduction electrons and holes at finite temperature and is directly proportional to system bandwidth. Shot noise varies with average power and is associated with photon detection statistics. By explaining these sources, the guide gives engineers a foundation for understanding why noise behavior changes with bandwidth, temperature, power level, and device architecture.
The eBook then compares two major noise figure measurement methods: the Y-factor or hot / cold-source technique and the cold-source or direct-noise method. The Y-factor method uses a noise source at the device under test (DUT) input to create hot and cold noise states, then calculates noise figure from the ratio of measured output powers. The guide explains why this method is widely used and where it has limitations, especially for extremely high or very low noise figure values. It also discusses analyzer-based noise figure measurements, cold-source measurements using network analyzers, and portable field measurements using handheld analyzers.
Designed for engineers working with receivers, low-noise amplifiers, converters, transistors, transmit / receive modules, and weak-signal systems, this eBook provides a practical introduction to noise figure fundamentals, measurement setup, device characterization, uncertainty reduction, and instrument selection. It is relevant for RF development, product validation, manufacturing test, field test, and engineering education teams that need to understand how noise affects weak-signal detection and how accurate noise figure measurements support better system-level sensitivity estimates.
何をお探しですか?