eBooks
Distributed, disaggregated digital transformation leaves no network element untouched. Cloud migration, software-defined wide area network (SD-WAN), data center upgrades, advanced cybersecurity capabilities, the Internet of Things, and application proliferation are examples of significant technology shifts. Organizations are embracing these shifts through digital transformation, which itself brings significant technical challenges.
The converged data center, along with the increasing importance of on-demand scale with virtualization in hyperscale data center networks, is shifting fundamental approaches to building these networks. New applications such as machine learning and artificial intelligence are changing how workloads use data center resources. Technologies such as Remote Direct Memory Access over Converged Ethernet version 2 (RoCEv2) and Media Access Control Security (MACsec) are being recast to deal with new problems like increasing storage workload transfer and the inability of IP-based encryption to keep up with modern data center traffic demands.
何をお探しですか?