Physical Layer Test System (PLTS)

技術概要

The Physical Layer Test System (PLTS) is the industry standard for signal integrity measurements and data post-processing tools for high-speed AI interconnects such as cables, backplanes, PCBs, and connectors.

 

Introduction

The Physical Layer Test System (PLTS) is the industry standard for signal integrity measurements and data post-processing tools for high-speed AI interconnects such as cables, backplanes, PCBs, and connectors. Today’s AI infrastructure demands ultra-reliable high-speed interconnects to support terabit-scale data throughput for applications such as machine learning, cloud computing, and autonomous systems. Ensuring signal integrity across interfaces like PCIe, Ethernet, DDR, USB Type-C, NVLink, HDMI, SATA, and Thunderbolt is critical for performance and compliance.

 

Many signal integrity laboratories around the world have benefited from the power of PLTS in the R&D prototype test phase and high-volume manufacturing phases. The terabit internet infrastructure demands multiport channel analysis to mitigate crosstalk issues that can cause bit errors. The new PLTS has now migrated to a powerful 64-bit application that enables deeper memory for large data files and achieves 16- or 32-port S-parameter measurements.

 

Why is Physical Layer Testing Required?

 

The next generation computer and communication systems now being developed will handle data rates of multiple gigabits/second. Many systems will incorporate processors and SERDES chip sets that exceed Gigahertz clock frequencies. New and troubling input/output issues are emerging as switches, routers, server blades, and storage area networking equipment moving toward 1.6 Tbps and 800 Gbps data rates.

 

Digital design engineers choosing chip-to-chip, chip-to-module and backplane technologies for these systems are finding signal integrity challenges that have not been encountered before.

 

Traditional parallel bus topologies have run out of bandwidth. As parallel busses become wider, the complexity and cost to route on PC boards increase dramatically. The growing skew between data and clock lines has become increasingly difficult to resolve within parallel busses.

 

The solution is fast serial channels. The newer serial bus structure has quickly replaced the parallel bus structure for high-speed digital systems. Engineers have been turning to a multitude of gigabit serial interconnect protocols with embedded clocking to achieve the goal of simple routing and more bandwidth per channel.

 

However, these serial differential interconnects bring their own set of problems. In order to maintain the same total bandwidth as the older parallel bus, the new serial bus needs to increase its data rate. As the data rate increases through serial interconnects, the rise time of the data transition from a zero-logic level to a one logic level becomes shorter.

 

This shorter rise time creates larger reflections at impedance discontinuities and degrade the eye diagram at the end of the channel. As a result, physical layer components such as printed circuit board traces, connectors, cables, and IC packages can no longer be ignored. In fact, in many cases, the silicon is so fast that the physical layer device has become the bottleneck.

 

With the aim of maintaining signal integrity throughout the complete channel, engineers are moving away from single-ended circuits and now use differential circuits. The differential circuit provides good Common Mode Rejection Ratio (CMRR) and helps shield adjacent PCB traces from crosstalk.

 

Properly designed differential transmission lines will minimize the undesirable effect of mode conversion and enhance the maximum data rate throughput possible. Unfortunately, differential signaling technology is not always an intuitive science.

 

Differential transmission lines coupled with the microwave effects of high-speed data have created the need for new design and validation tools for the digital design engineer. Understanding the fundamental properties of signal propagation through measurement and post measurement analysis is mandatory for today’s leading-edge telecommunication and computer systems.

 

The traditional Time Domain Reflectometer (TDR) is still a very useful tool, but many times the Vector Network Analyzer (VNA) is needed for the complete characterization of physical layer components.

 

There is a strong need for a test and measurement system that will allow simple characterization of complex microwave behavior seen in high-speed digital interconnects. In fact, many digital standards groups have now recognized the importance of specifying frequency domain physical layer measurements as a compliance requirement.

 

Many high-speed protocols have adopted the SDD21 parameter (input differential insertion loss) as a required measurement to ensure channel compliance (Figure 3). This parameter is an indication of the frequency response that the differential signal sees as it propagates through the highspeed serial channel. An example of a proposed SDD21 compliance mask is shown in Figure 1 for the Channel Electrical Interface (CEI) working group for the Optical Internetworking Forum (OIF).

 

A Single Test System Can Provide the Total View

As the combination of both time-domain and frequency-domain analysis becomes more important, the need for multiple test systems becomes difficult to manage. A single test system that can fully characterize differential high-speed digital devices, while leaving the domain and format of the analysis up to the designer, is a very powerful tool.

 

Keysight’s Physical Layer Test System (PLTS) is designed specifically for this purpose. PLTS has been designed specifically for signal integrity analysis. PLTS software guides the user through hardware setup and calibration and controls the data acquisition.

 

It automatically applies patented transformation algorithms to present the data in both frequency and time domains, in both forward and reverse transmission and reflection terms, and in all possible modes of operation (single-ended, differential, and mode-conversion).

 

A powerful virtual bit pattern generator feature allows a user-defined binary sequence to be applied to the measured data to convolve eye pattern diagrams. Next, highly accurate RLCG models can be extracted and used to enhance the accuracy of your models and simulations.

 

While PLTS is predominantly an R&D tool, a SCPI interface with a rich set of commands enables remote and manufacturing applications. Also, manufacturing applications benefit from the custom characterization report inside PLTS that allows users to document all multi-domain data required automatically.

 

PLTS Provides Design Confidence Through Complete Characterization

Physical-layer structures have increasingly become the bottleneck in high-speed digital system performance. At low data rates, these interconnects are electrically short. The driver and receiver are typically the biggest contributors to signal integrity.

 

But as clock speeds, bus speeds, and link speeds all push past the gigabit-per-second mark, physical-layer characterization becomes more critical. These interconnects become microwave transmission lines and need to be characterized carefully to avoid internet infrastructure failure.

 

Another challenge for today's digital designers is the trend to differential topologies. Fully understanding device performance requires analysis in all possible modes of operation.

 

Download the PDF to learn more about PLTS and high-speed signal integrity testing.