Make Accurate Lifetime Predictions for Battery Powered Devices

アプリケーションノート

The Challenge

It is no secret that health care costs are growing quickly. For example, U.S. health care inflation exceeded the general U.S. inflation rate in every year from 2005 through 2015 except 2009.[1] An ironic fact is that some of the cost is associated with infections picked up in healthcare facilities. The U.S. Center for Disease Control (CDC) says, “On any given day, about one in 25 hospital patients has at least one healthcare-associated infection.”