アプリケーションノート
ESD Considerations
A GaAs IC can be destroyed electrically by a static (or other) discharge through the device. Therefore, it must be handled so these effects cannot occur. Normal electrostatic discharge (ESD) preventive measures should be incorporated into all aspects of the storage, handling, and assembly of these devices. Specific measures to be taken should include:
In addition to ESD prevention measures, assembly equipment should be inspected for any power line transients that may couple into equipment that comes in contact with ICs.
何をお探しですか?