Webinars
Datacenter traffic is growing exponentially, driven by demanding applications like AI/ML Training, Cloud Computing, and Video Streaming. Photonic Integrated Circuits (PICs) have become an enabling technology in the rapid expansion of datacenter connectivity due to their lower cost, lower power consumption, small footprint, and high-speed performance.
One of the main challenges of utilizing PICs for datacenter applications is the design complexity associated with their integration into a fiber-optic communication system. Specifically, impairments stemming from the PIC may not be recognized until its performance validation in the application of interest. As a result, optimizing the PIC parameters in the context of the entire system is crucial to making informed decisions about technology choices and design alternatives.
In this tutorial, we explore the photonic design process at both the circuit and the system level. Join us to learn how to automate the design of PICs and simulate high-speed optical transmission systems using VPIphotonics Design Suite.
何をお探しですか?