Analyzing TDD Signal Timing with FieldFox

デモ

This video demonstrates how to use a FieldFox analyzer to examine the timing of a time division duplex (TDD) signal. Through a sequence of instrument screen views, it shows how to move from locating a signal in the frequency domain to observing its active and inactive intervals over time. The demonstration focuses on center frequency, zero span, sweep time, and burst trigger settings.

 

The video begins with a spectrum display showing a signal at approximately 1 GHz. A marker identifies the signal’s frequency, and the analyzer’s center frequency is set to match it. This establishes the frequency to observe before switching to a time-based measurement.

 

Selecting zero span changes the display from a spectrum across a frequency range to signal amplitude over time at the selected center frequency. The resulting trace reveals a repeating series of transmission bursts. Higher-level portions represent active transmission intervals, while lower-level portions show inactive intervals. These features make the signal’s intermittent behavior visible.

 

The demonstration then adjusts sweep time to examine the burst pattern at different time scales. A 15-millisecond sweep shows multiple repeating bursts, providing an overview of the timing pattern. Reducing the sweep to 3 milliseconds expands the display of individual bursts and the gaps between them. On-screen annotations identify an active transmission interval and an inactive interval, connecting the trace’s shape with the signal’s transmission behavior.

 

The next portion demonstrates burst triggering. The trigger settings include controls for trigger type, slope, delay, level, and position. The analyzer is configured for an RF burst trigger, and the trigger level is adjusted to −20 dBm. An on-screen message confirms successful burst trigger alignment. This step provides a timing reference for viewing the burst on the display.

 

Further sweep-time adjustments show the signal at 2-millisecond and 1-millisecond scales. The closer views make the transitions between active and inactive periods easier to inspect. A marker positioned at 500 microseconds provides a reference point on the time trace.

 

This short demonstration presents a practical sequence for analyzing TDD signal timing with FieldFox: locate and center the signal, select zero span, adjust sweep time, configure burst triggering, and inspect the transmission intervals. It illustrates how spectrum analyzer controls can reveal the timing structure of a pulsed RF signal.