Webinars
Caliptra is an open, standardized Root of Trust designed to support authenticated execution, protected key handling, secure boot, and firmware integrity in silicon used for servers and other critical infrastructure. As adoption grows across datacenter platforms, Caliptra is increasingly seen as a strong foundation for addressing security expectations that also matter under the EU Cyber Resilience Act (CRA), particularly in areas such as secure boot, secure updates, key protection, and system integrity.
Products that adopt Caliptra must complete a trademark audit before manufacturers can claim Caliptra use. In practice, many align that process with an OCP S.A.F.E. assessment to demonstrate independent verification of their Root of Trust implementation.
This webinar focuses on Caliptra trademark audits and how they intersect with CRA requirements and OCP S.A.F.E. reviews. Attendees will gain practical insight into the preparation needed to move through audit efficiently while meeting hyperscale and regulatory expectations.
何をお探しですか?