Case Studies
Cohere Technologies collaborates with Keysight on multi-UAV ISAC validation.
Validate sensing and communications under realistic, fast-changing radio conditions.
Cohere Technologies is collaborating with Keysight to validate sensing and communications for multiple unmanned aerial vehicles (multi-UAVs). Closely spaced moving targets create fast-changing, high-Doppler radio conditions that are difficult and costly to validate in the field. The collaboration combines Cohere’s delay-Doppler waveform technology with Keysight’s integrated sensing and communications (ISAC) emulation capabilities.
Cohere’s Multi-Waveform RAN program turns a commercial cellular base station into an integrated sensing and communications platform. It can detect, classify, and track drones while continuing to carry normal 5G traffic in commercial spectrum. Multi-UAV operations create fast-changing, high-Doppler radio conditions with many closely spaced moving targets.
Cohere combines its delay-Doppler waveform technology with Keysight’s expanded ISAC emulation capabilities to validate Zak-OTFS waveforms for multi-UAV use cases. Keysight brings sensing and communications scenarios into the lab through real-time RF channel emulation in PROPSIM, site-specific modeling, and automated test workflows. The solution supports hundreds of simultaneous sensing targets and massive Multiple-Input Multiple-Output (MIMO) testing, including large-scale antenna configurations for emerging 6G research.
The collaboration enables lab-based validation of Cohere’s Zak-OTFS waveforms for multi-UAV ISAC use cases. Keysight’s test and emulation capabilities enable Cohere to validate its physical layer against realistic channel and drone-target conditions before moving to field testing. Developers can evaluate sensing algorithms, waveforms, and wireless communications together under realistic, repeatable RF conditions.
The Multi-Waveform RAN program, funded by the DoD FutureG Office, turns a commercial cellular base station into an integrated sensing and communications platform that can detect, classify, and track drones while continuing to carry normal 5G traffic in commercial spectrum. Our multi-waveform physical layer runs on the open OCUDU software stack and supports both 5G OFDM and Pulsone™ Technology based on the Zak-OTFS waveform. Keysight’s test and emulation capabilities enable us to validate this physical layer against realistic channel and drone-target conditions before moving to field testing.
Cohere’s multi-UAV ISAC work requires sensing and communications to be evaluated together under demanding radio conditions. Its collaboration with Keysight brings Zak-OTFS waveform validation into a controlled, repeatable lab environment before field testing. Peng Cao, Vice President and General Manager, Wireless Test Group, Keysight, said: “Keysight is helping the 6G ecosystem accelerate innovation with greater confidence.
何をお探しですか?