Case Studies
With a modern Keysight Network Visibility Platform now supporting its BlueCat environment, the energy provider has a scalable foundation for the next phase of its network modernization strategy. Operations teams have assurance that performance and security tools are receiving complete, trustworthy traffic, resolving the operational complexity that limited previous investments.
As the organization continues expanding its network and security capabilities, the visibility architecture is positioned to scale alongside it, supporting additional sites, higher-speed links, and future monitoring and security initiatives without requiring a redesign of the visibility layer. The provider’s security team is also evaluating data loss prevention and other new tools to strengthen monitoring and asset discovery. The same visibility foundation is built to extend to these and future security and performance tools as they come online, feeding each one the same clean, reliable traffic without requiring the provider to rebuild or reconfigure the underlying architecture.
何をお探しですか?