レッスン
Quantum computing is gaining attention for its ability to solve complex problems that regular computers struggle with. In this journey, instruments like the DC bias source play a crucial role, especially for flux-tunable superconducting qubits and silicon spin qubits. In this video, we will dig into quantum computing development, focusing on the role of Source Measure Units, or SMUs, in controlling multiple qubits with low-noise precision bias.
There are two main challenges faced in using DC power supplies for this:
1st Challenge:
Voltage fluctuations from DC power supply noise and environmental interference through long cables can cause qubit decoherence. Qubits are super sensitive, and even small changes in DC bias voltage can mess up their quantum state, leading to information loss. This is called decoherence, and it makes qubit control less precise.
In the quantum world, qubits exist in a superposition of states, representing both 0 and 1 simultaneously. This unique property makes them exceptionally powerful for certain computations. However, it also makes them incredibly sensitive to external influences. The challenge arises when DC power supply noise and environmental interference introduce voltage fluctuations that disturb the delicate balance of the qubit's superposition.
Even the tiniest variation in voltage can cause the qubit's quantum state to waver, leading to decoherence. When decoherence occurs, the qubit loses its special quantum properties, making it less reliable for computations. This is a significant challenge in quantum computing because maintaining the integrity of qubit states is crucial for accurate and reliable quantum information processing.
Voltage fluctuations disrupting qubit coherence are deeply rooted in quantum systems' fundamental nature. The challenge is not just preventing external disturbances but also developing tools and technologies that can shield qubits from these disturbances, ensuring stable and coherent quantum states for reliable computational processes.
2nd Challenge:
Secondly, as quantum computers grow with more than 100 qubits, there's a need for lots of power supplies, and that takes up a ton of space. Each qubit needs its own independent DC bias, and housing hundreds of general power supplies becomes a logistical challenge.
As quantum computers progress beyond the 100-qubit milestone, the demand for independent DC bias for each qubit grows substantially. Each qubit requires its own dedicated power supply to ensure precise control and manipulation. This necessity creates a logistical challenge in terms of physical space within quantum computing laboratories.
The need for substantial space arises from the requirement to house several hundred general power supplies, each catering to the unique needs of individual qubits. This spatial challenge not only impacts the physical layout of the lab but also raises practical concerns about efficient management, accessibility, and maintenance of the equipment.
To address this challenge, there is a growing emphasis on developing compact and efficient power supply solutions that can cater to the individual requirements of each qubit while minimizing the overall footprint. Streamlining the power supply infrastructure is essential for the scalability of quantum computing endeavors, allowing researchers to expand their quantum systems without being hindered by space limitations.
Dealing with voltage fluctuations and spatial limitations in DC bias sources for quantum computing is crucial for progress. Keysight Technologies, with its advanced Source Measure Units, aims to provide simple yet powerful tools for the quantum computing community to tackle these challenges and take quantum computing to new heights of reliability and capability.
In this course video, we will cover all the challenges mentioned above in great detail, including steps to provide clean DC bias voltage for multiple qubit control while ensuring all the above challenges are addressed accordingly. We will also cover some tips and tricks to further minimize the effect of voltage fluctuations to prevent qubit decoherence.
何をお探しですか?