How-To Videos
Identifying the root cause of failed charging sessions is challenging without observing or analyzing the communication channel between an EV and EVSE. Having limited debugging capabilities can make issue resolution time-consuming, increase dependence on manufacturing support, and cause safety risks.
In this demo, we will show how a protocol trace viewer enables seamless observation of the CCS communication channel between an EVSE and an EV and decode the CCS charging protocol. With this information, you can start debugging easier and quicker.
何をお探しですか?