Fox Hunt: Microwave Face-Off

ビデオ

In this video, we explore the fascinating world of microwaves, showcasing the capabilities of two microwaves and a FieldFox handheld analyzer. Through real-time spectrum analysis (RTSA), we analyze the radiation coming from each microwave and push the limits of signal transmission by testing the walls of the microwave with one FieldFox as a transmitter and another as a receiver. We also test if a phone will still ring in a microwave by setting the FieldFox to 751 MHz to see the LTE signals. The video provides an engaging and informative demonstration of the hidden powers of microwaves.