Using Software In The Loop (SIL) and Hardware In The Loop (HIL) for ITS Applications Test

ビデオ

Testing Application Layer performance is complex so testing in a Software In The Loop (SIL) environment will enable developers to test approx 80% of the functionality of a system. However, when real RF HW is introduced several factors come into play which need to be tested. Comparing KPI's in a SIL and then a HIL environment allows these factors to be tested.