Testing EV Batteries at the Cell, Module, and Pack Levels

ビデオ

Electric vehicle (EV) batteries come in different form factors: at the individual cell level, these may be cylindrical cells, or more powerful pouch and prismatic cells. These cells are then assembled into modules, which are in turn, connected to form battery packs, and then assembled into the vehicle chassis. Join our Keysight battery test expert to learn how different battery test parameters at each stage guide how the battery will eventually perform in the EV.