The Importance of Lossless Network Visibility

白書

Why Lossless Visibility Matters

IT security and analytics tools are only as good as the data they are seeing. IT’s fundamental challenge is to ensure that the infrastructure behind these tools delivers applications that are reliable, fast, and secure. This means that IT needs total visibility of the network. With the current level of network security threats and a complete dependence by the business on the data network, you cannot afford partial network visibility. You need lossless visibility.

According to a Cost of Data Center Outages study conducted by the Ponemon Institute, the average cost of a network outage is $7,793 per minute.1 When the network is down or impaired, minutes matter. This is especially important as global IP traffic levels will triple from the 2017 level of 122 EB per month to 396 EB per month in 2022, 2 according to the Cisco Visual Network Index, Forecast and Methodology: 2017-2022. Better network visibility can improve mean time to repair by helping pinpoint problems.

A visibility architecture helps eliminate these concerns by organizing and integrating your monitoring strategy with your security architecture and problem resolution processes. However, there are three fundamental items to consider when creating a visibility architecture:

  • Performance matters when you are trying to control costs
  • Missing data is an unnecessary security risk
  • Missing data leads to longer and more costly troubleshooting efforts

So, how do you eliminate these issues?