白書
The CIO and CISO Security Challenge
As daily news stories continue to document, enterprises are struggling with how to prevent security breaches to their networks. Not only do breaches affect the company brand, but economic losses continue to mount, as well.
In the current business climate, it is not a question of if your network will be attacked, but when it will be attacked. And, the real question is how quickly can you respond to the threat and recover. In fact, these are two of the questions that keep chief information officers (CIOs) and chief information security officers (CISOs) up at night:
Because of these realities, a new paradigm shift in network security is needed. While security defenses still need to be maintained, there has to be at least equal, if not greater, effort placed on recovering the network back to a normal, safe state as quickly as possible. This philosophy is called security resilience.
何をお探しですか?