eBooks
Introducing Wi-Fi 6/6E
Wi-Fi is a mission-critical technology. People and businesses depend on it for fast, reliable connections to the internet or other devices within an environment. That’s why every new Wi-Fi standard generates a lot of excitement. And the truth is, Wi-Fi 6 delivers.
Wi-Fi 6 offers higher capacity, faster speed, and lower latency. But more importantly, it enables Access Points (APs) to support more clients in dense environments through efficient spectrum use. That’s a game changer. Earlier iterations of Wi-Fi allow all parties to contend for the medium. As more and more devices access the networks, medium contention presents a genuine challenge. Wi-Fi 6 addresses this challenge by giving control of the medium to the AP. The AP can schedule multiple clients to transmit or receive concurrently, using orthogonal frequency-division multiple access (OFDMA) with allocated resource units.
O que você está procurando?