HP8920 Mode on the M8920A

Notas de Aplicação

HP8920 Compatibility Mode

 

The M8920A PXIe Radio Test Set can be used to replace legacy HP8920 RF Communication Test Sets in an automated test environment with minimal or no modification to the currently used measurement software.

• Run legacy programming codes using newer SCPI-based instruments without code modification

• Reduce ATE system investment with M8920A PXIe Radio Test Set