Choosing a System Power Supply for Mobile Device Testing

Notas de Aplicação

Pulsed battery drain currents, regulated charge currents, and remote DUT (Device Under Test) fixtures, dictate the need for specialized power sourcing, loading, and measurement capabilities for testing mobile communications devices. Many of these capabilities are not available in general-purpose system power supplies. This guide will assist the test system designer in selecting a system power supply by properly evaluating test system and power supply needs that are unique to the application and not immediately obvious. In this way, many problems likely to arise in production can be avoided.