Notas de Aplicação
When it comes to measurement instrumentation, one size does not fit all. What instrument a user selects is often dictated by his/her evolving test needs or need to meet key objectives. That’s one reason why modular test systems have become so compelling; they consist of hardware instrument building blocks and associated drivers that can be combined to create virtually any type of instrument the user might need. Instruments can consist of a single module or multiple modules that can be combined to create a multi-module instrument (MMI).
O que você está procurando?