Tailgate Sensor Detection on i3070 Inline ICT Testers

Notas de Aplicação

With broad adoption by electronics manufacturers looking to automate their board test strategy, Keysight Technologies, Inc. continues to innovate with its i3070 Inline In-Circuit Test (ICT) solution. New features have been recently introduced to improve customer experiences in terms of safety and productivity. One of the latest features is detection of tailgating boards. This innovative technique can eliminate the risk of printed circuit board assemblies (PCBAs) being damaged if the upstream system should fail to move the PCBA properly due to any sensor malfunction. Another potential error which could arise is if the operator manually loads a PCBA, causing two PCBA boards to pile up back to back.