InfiniiVision 2000 X-Series Oscilloscope

Visão Geral Técnica

Quick Demo Guide

Getting started

The Auto Demo and App Demo modes allow you to demonstrate oscilloscope features using internally generated signals. For these demos, probe the front panel Demo 1 terminal using Channel 1 and probe the front panel Demo 2 terminal using Channel 2 as shown in the connection diagram above.

Using the “Auto Demo” mode

Auto Demo shows:

  •  Fast waveform update rate
  •  Mixed signal oscilloscope
  •  Segmented memory acquisition– Mask testing
  •  WaveGen function generator

Use the “Auto Demo” mode to quickly demonstrate key features and capabilities of the oscilloscope in two easy steps.

App Demo shows:

– Serial bus (all available protocols)

– Digital voltmeter (DVM)

Use the “App Demo” mode to quickly demonstrate some of the scope’s more advanced measurement applications and options in two easy steps.

In addition to the “Auto Demo” mode, the InfiniiVision Series oscilloscopes also provide a wide array of additional built-in “Training Signals” that can be selected in order to demonstrate some of the new and more advanced triggering and automatic measurement capabilities of the InfiniiVision 2000 X-Series oscilloscope.