WiMAX Signal Analysis: Troubleshooting Symbols – Part 3

Notas de Aplicação

This application note is intended for engineers who are familiar with the IEEE 802.16-2004 (WiMAX) physical layer standard and wish to improve their measurement understanding and capabilities using a vector signal analyzer (VSA). This application note from Keysight Technologies, Inc. will provide information on how to improve WiMAX signal analysis and includes measurement tips when designing and troubleshooting a new or an existing product. In order for the RF engineer to successfully test and troubleshoot a WiMAX device, a well-organized approach to the signal analysis will yield the greatest level of understanding and reliability in the measurement. This application note is one part in a series that provide the framework for the preferred measurement approach that includes frequency and time measurements, digital demodulation, and analysis of the advanced functionality within the WiMAX physical layer definition. If you are familiar with the 802.16- 2004 standard but not necessarily familiar with WiMAX measurements, you may find reading all the application notes in this series very useful for expanding your knowledge of testing and troubleshooting this complex signal.