SPICE Model Verification in IC-CAP Model Generator

Notas de Aplicação

Quality assurance (QA) checks are essential in the device model extraction flow. Modeling engineers must rigorously evaluate the extracted models through QA checks to assure the quality of the final model. This process is essential not only to ensure that device behavior matches actual measurements but also to verify model consistency under different simulation conditions and environments.

 

The newly added Model Generator QA is a highly effective tool developed to streamline the entire device modeling workflow. This tool greatly simplifies the traditionally time-consuming and labor-intensive QA flow for modeling engineers, allowing them to perform fast and accurate quality assurance while maintaining confidence in the simulation results.

 

This application note will show how Model Generator QA can streamline Spice Model Verification for modeling engineers.