Programming Examples for PZ2100 Using Command Expert

Notas de Aplicação

This application note provides a comprehensive guide for utilizing Keysight's Command Expert tool with the PZ2100 Source Measure Unit (SMU). The PZ2100 offers high-precision voltage, current sourcing, and simultaneous measurement capabilities, making it ideal for various research, development, and manufacturing applications. The Command Expert tool streamlines instrument control by integrating commands, documentation, syntax checking, and execution within a user-friendly interface. This guide includes instructions for installing PZ2100 command sets, connecting to the instrument, and running programming examples for various measurement scenarios such as DC spot, sweep, pulsed measurement, and external triggering. Each programming example includes input parameters, timing charts, and tips for efficient usage. Additionally, the note outlines integration with BenchVue for enhanced evaluation and debugging processes.