Testing Defense and Aerospace Systems with Keysight Eggplant Test

Notas de Aplicação

Keysight Eggplant Test (hereafter called “Eggplant”) can be used to automate tasks in a wide variety of industries, including Defense and Aerospace. The Defense and Aerospace sector uses diverse systems, from radar tracking to aircraft avionics to GIS and location mapping. You can use Eggplant to test any of these systems. Eggplant’s innovative solution combines computer vision and robotics to mimic a user’s view of the systems, providing invaluable visual verification testing without manual intervention. As an example, this application note illustrates how to use Eggplant to model a GIS system. GIS systems can be challenging to test because their use cases and data are specific to each customer, and customers' data change. This application note includes the following sections:

  • Setting Up Eggplant
  • Modeling a GIS System
  • Running a Model