Better Limits Setting with PAT Limit Recommendation

Notas de Aplicação

Part Average Testing (PAT) is a method that uses robust statistics to detect outliers, which is widely used in the automotive industry. It was developed based on standards specified in the guidelines from Automotive Electronics Committee (AEC).

 

PathWave Manufacturing Analytics (PMA) uses PAT to detect PAT anomalies and PAT Limit recommendations. This article will go over the PAT recommendations module in more detail.