Notas de Aplicação
In order to make automation test more efficient, the SCPI-Recorder is now available in X-Series measurement applications. It covers several complex measurement scenarios, such as 5G NR, Digital Demod, Custom OFDM etc. You can utilize this powerful tool to speed up your development of test automation systems. This demo guide shows you how to find and show the parameter related SCPI command quickly instead of hunting around the manual to find right SCPI command and exact syntax, generate SCPI script automatically, and playback SCPI commands to setup complex measurement easily.
SCPI List and Script Generation
SCPI-Recorder in the system settings provides you a SCPI list of your manual operation in the test. A SCPI list may consist of several commands in their chronological order of execution. Or it may consist of all SCPI commands needed for a certain functional test but not necessarily in the advisable order of their execution. Thus, there are two modes to create the SCPI list. One is called automatic SCPI List recording via enabling the button called ‘Continuous SCPI Recording’. Another one is called manual SCPI list recording via disabling the ‘Continuous SCPI Recording’ and pressing the button called ‘Add to SCPI Recorder’.
O que você está procurando?