Notas de Aplicação
Time is Critical for IoT Success
The internet of things (IoT) is growing quickly, and it presents numerous opportunities to improve people’s lives in applications such as smart cities, environmental monitoring, smart health care, smart agriculture, smart logistics, and more. In addition, the IoT presents profitable business opportunities, especially for companies that can bring devices to market quickly to gain market share and capture the highly profitable early adopter phase of the market cycle.
Why OTA Signaling Test is Important
One key to getting products to market quickly is to get quantitative measurements of how the device operates as the customer will experience the operation. This means that it is not enough to do a simple golden radio test that only ensures basic connectivity. You also need to know the power levels at which the device operates and to measure parameters such as packet error rate, advertising interval, throughput, and receiver sensitivity. It is also important to perform OTA testing rather than connected testing to ensure that the entire signal path, including the antenna, is performing properly.
O que você está procurando?