Solution Briefs
Multivendor and Distributed Cloud 5G Core Keysight Visibility Platform
5G Visibility for Multi vTAP Network Function Providers
Mobile network operators face challenges gaining complete 5G network visibility
As the world moves to 5G, the number of mobile subscribers is increasing rapidly. Subscribers use mobile devices also for more complex and substantial tasks than before including 4K video like Netflix or Amazon and social streaming applications such as YouTube, Vimeo, Facebook and Instagram.
Meeting the low latency needs of 5G requires the transformation of the mobile core network. A distributed and disaggregated environment gets user content to the edge where it can be quickly accessed by the mobile phone subscribers. Still, this is only the start of complexity that is happening with the 5G network transformation.
In addition, new approaches to segmenting traffic such as network slicing must be visible to the monitoring platform, as well as the new 5G architectures need to be designed with the ultimate goal of becoming a true software defined network.
O que você está procurando?