Solution Briefs
Cynerio and Keysight: Reduces Cyber Risk for IoMT Devices
Overview
Security in a healthcare environment is crucial because lives and sensitive data are on the line. Many hospitals and other medical facilities are taking advantage of ubiquitous wireless networking to roll out connected medical devices to help diagnose and monitor patient health. These devices are knowns as internet of medical things (IoMT). Connected medical devices, however, are frequently opaque to conventional IT management tools, making them nearly impossible to protect and secure.
What’s needed is a security tool that not only understands medical devices and the IoMT ecosystem but can also determine the function of IoMT devices and the context of their behavior without disrupting patient care or network operations. That way you can prioritize risks based on their potential impact on patient safety and patient care. Cynerio’s security solution, working together with the Keysight Network Visibility solution, provides the healthcare-driven behavior analysis necessary to give IT teams insight into IoMT networks.
O que você está procurando?