Addressing Wi-Fi Measurement Challenges with a Multi-channel Test Instrument

Notas de Aplicação

Evolution of Wi-Fi Technologies

 

Wi-Fi is one of the dominant wireless technologies in the world and its success rests on a solid foundation established over the last 20 years. Wi-Fi technologies have evolved at a fast pace while providing continuity with full backwards compatibility.

 

As the first wireless access technology that used unlicensed spectrum, Wi-Fi has gone through several generations to meet increasing requirements in data throughput and performance expectations in terms of speed, latency, and reliability.