Control Tower Stack Light

Notas de Aplicação

Introduction

Inline equipment’s are functioning automatically without human intervention on the manufacturing floor. However, when a problem occurs how does the equipment attract attention from its human operators? The System Tower Light also known as signal tower light installed on top of the automated i3070 Inline In-Circuit Test (ICT) in a printed circuit board assembly (PCBA) manufacturing floor is a straightforward way to address this. It provides visual and clear indicators of the ICT status or operation condition to the manufacturing support personnel.

 

Overview

During ICT Auto mode, the Programmable Logic Control (PLC) on the i3070 inline ICT controls the tower light color (Figure 1) to indicate the system state or condition. This application note describes how to use the i3070 test plan to change the tower light indicator based on user preference during production.