From Standard Ethernet to Automotive Ethernet

Flyer

An Automotive Ethernet Tip  

Standard Ethernet

Standard Ethernet, BASE-TX has proven itself as a secure transfer medium that can handle large amounts of data in internet infrastructure companies and high-speed data centers, as well as offices, and homes. The advantages of Ethernet — multi-point connections, higher bandwidth, and low latency — are attractive to automotive manufacturers. However, traditional Ethernet did not meet the EMI/RFI requirement set by the OEMs and is interference-sensitive, making it less than ideal for use in the harsh conditions in a vehicle.