小冊子
6G Research in D-Band
Building upon Keysight’s leadership and expertise in 5G, we can also help you make the vision of 6G a reality. 6G research addresses a multitude of frequency bands, frequency bandwidth, and waveform types. The potential 6G frequency bands include D-band (110-170 GHz), G-band (140-220 GHz), and H-band (220-330 GHz). Some recent 6G research paper claim that the millimeter bands (mmWave) – specifically D-band – are the channels that 6G technology will travel.
Noise Figure Measurement
Noise figure is one of the fundamental parameters that differentiates one system, amplifier, or transistor from another. N9069EM0E noise figure measurement application offers development engineers a simple tool to make accurate and repeatable noise figure measurements.
It allows engineers to rapidly measure any one of the following in their test racks:
1. noise figure/factor
2. gain
3. effective temperature
4. Y-factor
5. hot/cold power density
By using the signal analyzer with a down-converter and a noise source, it can quickly determine the noise of the device under test working in D-band.
何をお探しですか?