Atlassian JIRA Template Injection Code Execution

Strike ID:
E19-7o911
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2019

Description

This strike exploits a remote code execution in the JIRA Template. The vulnerability is due to improper sanitization of user input which is passed to the application via the ContactAdministrators and SendBulkMail actions. A remote authorized attacker can exploit this vulnerability by sending a crafted request to the target server. Successful exploitation results in remote code execution on the target server.

CVE