Converts 15-pin D-sub pulse I/O on the PNA-X’s rear panel to the coaxial SMB male connectors for better connectivity

HIGHLIGHTS

The Keysight N1966A pulse I/O adapter converts 15-pin D-sub pulse I/O on the PNA-X’s rear panel to the coaxial SMB male connectors for better connectivity. It contains input to receiver IF gates (for one reference and four test receivers), output from each of four internal pulse generators, RF signal pulse modulation drive input, and trigger input for the internal pulse generator timing.

For more information about cable and accessories for use with network analyzers, please visit Network Analyzer Accessories.

Amplie as Capacidades

Want help or have questions?