Choose a country or area to see content specific to your location
Notas de Aplicação
Introduction
Useful for high-temperature applications, newly developed high-entropy alloys (HEA) exhibit superior mechanical properties at high temperature when compared with conventional superalloys or structural ceramics [1]. The term high-entropy is associated with the stable solid-solution formation phase resulting from high configurational entropy [2]. However, presence of multi-phase microstructures in some HEA compositions indicate that factors such as mixing enthalpy and hence solubility of elements may also be predominant when controlling segregations during solidification, therefore promoting multi-phase structures. Due to the equimolar presence of several elements in the alloying system, mechanical properties at high temperature are influenced by the diffusion rate of each element in multi-phase systems.
*Indicates required field
Thank you.
Your form has been successfully submitted.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
*Indicates required field
Thank you.
A sales representative will contact you soon.